LTE TDD
For Waveform Playback (ARB) capability.
The Test Model button is displayed in the toolbar when the Downlink node is selected for a Basic TDD carrier.
Configures the downlink with an E-UTRA Test Model (ETM). One-shot action command (no query).
Comma-separated key:value argument; keys optional (omitted keys use preset defaults).
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:CONFig:TEST "<string>" |
|
SCPI Example |
RADio:LTETdd:WAVeform:CCARrier1:DLINk:CONFig:TEST "TestModelType:ETM11,SystemBandwidth:B10M,WaveformGenerationLength:SLOT2,SpecialSubframeConfig:8,UplinkDownlinkConfig:3" |
|
Notes |
Comma-separated key:value. Keys: TestModelType (ETM11|ETM12|ETM2|ETM2A|ETM31|ETM31A|ETM32|ETM33 + BC3CS3 variants), SystemBandwidth (B1M4|B3M|B5M|B10M|B15M|B20M), WaveformGenerationLength (SLOT1…SLOT14), SpecialSubframeConfig (0–8), UplinkDownlinkConfig (0–6). |
|
Preset |
N/A |
|
State Saved |
No |
|
Initial S/W Revision |
A.20.01 |